Technical FAQs

Ask a Question

BMXNOR0200H firmware version 1.7

Title
BMXNOR0200H firmware version 1.7
 
Issue
BMXNOR0200H firmware version 1.7
 
Product Line
M340, BMXNOR0200H
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The M340 BMXNOR0200H firmware version 1.7 that resolves the M340 Web Server Vulnerability issue (SEVD-2015-344-01).
Was this helpful?
What can we do to improve the information ?