Technical FAQs

Ask a Question

Is SymmetraMW native device in Power Monitoring Expert 8 for Date Center Edition and is there a default Vista diagram for this particular UPS?

Issue
Is SymmetraMW native device in Power Monitoring Expert 8 for Data Center Edition and is there a default Vista diagram for this particular UPS? 

Product Line
Power Monitoring Expert 8.x DC

Cause 
User would like to know if SymmetraMW driver is natively supported in PME 8 DC and is there a default vista diagram or not. 

Environment 
Adding SymmetraMW in PME 8.x DC 

Resolution
Yes, the SymmetraMW is a native device in a PME 8 for Data Center edition install. However, there is no default Vista diagrams explicitly for this particular UPS.

There is, however, a generic UPS diagram that can be used: <PME install directory>\Power Monitoring Expert DC Ed\config\diagrams\ud\DataCenter\Equipment\Equipment_Details_IT_UPS.dgm

For example: 
C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert DC Ed\config\diagrams\ud\DataCenter\Equipment\Equipment_Details_IT_UPS.dgm

NOTE: For all other PME version (like PME 7.2.2), there is custom driver installer which can be obtain by contating PowerLogic Technical Support. 
Was this helpful?
What can we do to improve the information ?