Technical FAQs

Ask a Question

Can the TMH2GDB display floating point numbers?

No. The TMH2GDB does not support floating point. The following Object Types are supported. 
These memory objects are available:
 System bit (%S)
 System word (%SW)
Memory bit (%M)
Memory word (%MW)
Constant word (%KW)
Memory double word (%MD)

These I/O objects are available:  
Input bit (%I)
Output bit (%Q)
Input word (%IW)
Output word (%QW)
Input status word (%IWS)
Output status word (%QWS)
Was this helpful?
What can we do to improve the information ?