Technical FAQs

Ask a Question

Is it possible to commission a Lexium SD328A using Lexium CT via CAN ?

No, the commissioning tool Lexium CT does not support connection to Lexium SD328A via CAN.
You must use the RS485 port to connect to the SD328 drives when commissioning the drive with Lexium CT
Was this helpful?
What can we do to improve the information ?