Technical FAQs

Ask a Question

Manufacturer information on the M221 analog input connector

Issue:
Manufacturer information on the M221 analog input connector

Product Line:


Environment:


Cause:


Resolution:
The manufacturer of the connector is JST.  See attached catalog of the connector or below webpage.

http://www.jst-mfg.com/product/pdf/eng/eXA1.pdf

The connector part numbers that could be used are either XAP-04V-1  or  XARP-04V.
Was this helpful?
What can we do to improve the information ?