Technical FAQs

Ask a Question

Does Schneider Electric offer a direct replacement for ILS1B573S1338 with ID number of 66106390010 ?

No, the Lexium Integrated Drive type ILS1B573S1338 with ID number of 66106390010 is an OEM specific model and can not be ordered directly from Schneider Electric.
ILS1B573S1338 with ID number of 66106390010 is a proprietary model and therefore you must contact the OEM machine builder for spare motors of this type.

The ILS1B573S1338 with ID number of 66106390010 has a 32:1 gearbox, which is not available is our standard catalog offer.
The ILS1B573S1338 also comes with industrial connectors.

Please contact the OEM machine builder to attain spare motors of type ILS1B573S1338 with ID number of 66106390010
Was this helpful?
What can we do to improve the information ?