Technical FAQs

Ask a Question

What is the flammability rating of the M340 PLC?

The M340 is compliant with the following standards. UL 746C, UL 94
 Electrical qualities and self-extinguishing capacity of insulating materials: .
 
Was this helpful?
What can we do to improve the information ?