Technical FAQs

Ask a Question

What is the part number for spare connectors for the motor power connection on the Berger Lahr D902, I902, WD3-004, WD3-008, WDP3-014 and WDP3-018 drives ?

All of the Berger Lahr legacy 3 phase stepper drives use the same 4 position motor power connector.
This connector is a product of Phoenix Contact and uses the Phoenix Contact part number of 1825336
Spare connectors of this type can be purchased from any of the distributors of Phoenix Contact products.

Here is the full description of the product as found on the Phoenix Contact web-site... Printed-circuit board connector - IC 2,5/ 4-STF-5,08 - 1825336

Additional data can be found here > https://www.phoenixcontact.com/online/portal/us?uri=pxc-oc-itemdetail:pid=1825336&library=usen&pcck=P-11-02-11&tab=1

 
Was this helpful?
What can we do to improve the information ?