Technical FAQs

Ask a Question

What are the part numbers for the Magelis GTO IP67 rated covers

Issue:
What are the part numbers for the Magelis GTO IP67 rated covers

Product Line:
HMIGTO, IP67 covers

Environment:


Cause:


Resolution:
Below are the part numbers for the HMIGTO IP67 covers:
HMIGTO1300/1310     HMIZECOV1
HMIGTO2300/2310     HMIZECOV2
HMIGTO3510/4310     HMIZECOV4
HMIGTO5310/5315     HMIZECOV5
HMIGTO6310 /6315    HMIZECOV6
Was this helpful?
What can we do to improve the information ?