Technical FAQs

Ask a Question

Preventa XCS - 4-wire cable evolution in the XCSDMP, XCSDMC and XCSDMR magnetic switches

Please note that, since date code 4515 in november 2015 (marking on the product), all the XCSDMP, XCSDMC and XCSDMR magnetic switches using 2 contacts and supplied with an electrical cable 4 wires, have a central element in white polypropylene (PE) to improve the quality of the cable in the manufacture process. Such cable evolution does not change the cable jacket diameter and the cable performances. The 3 contacts XCSDMP switches had such provision since their launch.

Was this helpful?
What can we do to improve the information ?