Technical FAQs

Ask a Question

Osisense XC - Rod lever ZCKY439057 datasheet

The rod lever ZCKY439057 is a special ZCKY59 polyamide rod lever with a longer rod. It is a round rod lever thermoplastic Ø6mm length =300mm, instead of 200mm for the standard ZCKY59 lever. Logistic situation in 2016 : available to order under the ZCKY439057 reference without any restriction. It is a product manufactured to order.

Was this helpful?
What can we do to improve the information ?