Technical FAQs

Ask a Question

Can the ACE850 be used to communicate with both IEC61850 and Modbus TCP/IP simultaneously?

Issue    
Customer would like to use both IEC61850 protocol and Modbus TCP/IP simultaneously.

Product Line    
SEPAM, ACE850TP, ACE850FO

Environment    
Communications over network

Resolution  
The ACE850 communication module can be used for simultaneous communication of IEC61850 and Modbus TCP/IP protocols. This procedure is supported and recommended.



 
Was this helpful?
What can we do to improve the information ?