Technical FAQs

Ask a Question

How do I interperate the 9th word in the IO Map for the 140ACI03000 ?

Words 1-8 will offer the current analog input values for channels 1-8 . The 9th word will provide the status of each channel on the 140ACI03000.
Status for the eight input channels are displayed in the low byte of word nine, the high byte is not used and should be ignored for the 140ACI03000.

 %IWn.0
  xxxx xxxx nnnn nnnn  

 %IWn.0 or LSB = Channel 1 status: 0 = healthy and in range, 1 = broken wire or under voltage
 %IWn.7  = Channel 8 status : 0 = healthy and in range, 1 = broken wire or under voltage


R-71117
 
Was this helpful?
What can we do to improve the information ?