Technical FAQs

Ask a Question

Can the M241 read the Average Current from a LULC08 Tesys U via CANopen?

You can read the Average motor current from a LULC08 via CANopen. 
PDO,  2004:11 Average Motor current.

 
Was this helpful?
What can we do to improve the information ?