Technical FAQs

Ask a Question

What is the MTBF for the Magelis HMISTU855?

-LCD and touch panel of STU655/855 is 50,000 hours

-HMISTU655/855 is 2,087,918 hours without LCD screen
Was this helpful?
What can we do to improve the information ?