Technical FAQs

Ask a Question

Osisense XZ - XSZCD121Y, XSZCD122Y, XSZCD123Y pre-wired M12 4-pin connector 90° replacement

The XSZCD121Y (2m), XSZCD122Y (5m), XSZCD123Y (10m) pre-wired M12 4-pin connector 90° with LEDs for PNP DC sensor association, can be respectively replaced by the XZCPV1340L2 (2m), XZCPV1340L5 (5m), XZCPV1340L10 (10m) equivalent cabling accessory, PVC cable. Attached :
- picture of the XSZCD121Y cable, and XSZCD12*Y details,
- XZCPV1340L2 data sheet.
                       
 
Was this helpful?
What can we do to improve the information ?