Technical FAQs

Ask a Question

What is the bore diameter of the output element on Lexium Integrated Drives with a worm gear type gearbox ?

The worm gear has a bore diameter of 12mm with a fit tolerance of F8

This dimension is the same for all worm gear gearbox's regardless of the ratio.

See attached drawing
Was this helpful?
What can we do to improve the information ?