Technical FAQs

Ask a Question

Osisense XZ - XSZCD1512Y pre-wired M12 5-pin connector 90° replacement

The XSZCD1512Y pre-wired M12 5-pin connector 90°, can be replaced by the XZCPV1264L5 equivalent cabling accessory, PVC cable 5m length (grey color). Attached the XZCPV1264L5 data sheet. The XSZCD1512Y is the 5m cable lenght version of the XSZCD1511Y reference in 2m cable lenght.
Was this helpful?
What can we do to improve the information ?