Technical FAQs

Ask a Question

Osisense XZ - XSZCD112Y pre-wired M12 4-pin connector 90° replacement

The XSZCD112Y pre-wired M12 4-pin connector 90°, can be replaced by the XZCPV1241L5 equivalent cabling accessory, PVC cable 5m length. Attached :
- picture of the XSZCD112Y cable,
- XZCPV1241L5 data sheet.

Description of the XSZCD112Y pre-wired M12 4-pin connector 90° : It is in fact the XSZCD111Y cable in 5m cable length version.
FEMALE; SINGLE KEYWAY; 90 DEG CONNECTOR; 4 POLE; WIRE CODE 1-BROWN 2-WHITE 3-BLUE 4-BLACK; PVC JACKET CABLE; YELLOW; LENGTH 5 M; APPLICATION SENSOR

Was this helpful?
What can we do to improve the information ?