Technical FAQs

Ask a Question

Osisense XC - ZCD28 (2NO contacts slow break) contact diagram

We can communicate on the fact that the XCKP, XCKD and XCKT limit switches have the same contact adjustement for the identical function, using the same head. The ZCT28P16+... contact diagrams are published into the Osisense XC catalogue. Find attached the ZCD28 catalogue pages with contact diagrams (partial) by analogy with the ZCT28. It is the same answer for the ZCP28+... limit switches. Please note that such contact body (not positive opening operation) cannot be used in a safety chain solution.
Was this helpful?
What can we do to improve the information ?