Technical FAQs

Ask a Question

Can I move the AlarmSummary cursor UP and Down in Vijeo Designer from the PLC?

You can write a script action control by PLC variables to move the cursor UP and DOWN.

Moves Alarm Summary DOWN by 1 row and return value 0 if no errors.
Msg_State.write(AlarmSystem1.cursorDown(0));  

Moves Alarm Summary UP by 1 row and return value 0 if no errors.
Msg_State.write(AlarmSystem1.cursorUp(0));  
Was this helpful?
What can we do to improve the information ?