Technical FAQs

Ask a Question

Does the 140NOE77101 support the NTP service?

Title
140NOE77101 does not support the NTP service
 
Issue
140NOE77101 does not support the NTP service
 
Product Line
140NE77101
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
The 140NOE 77101 does not support the NTP service. The NTP Service is in configuration Model Family but only supported by 140NOE 77111.
Unity 11 does indicate an error when you try to build the project and the NTP service is set to yes with a 140NOE77101 module.

 
Was this helpful?
What can we do to improve the information ?