Technical FAQs

Ask a Question

Can the BME XBP **00 Ethernet backplane be used as an extension rack in the M580 architecture?

Yes, you can use this type of backplane as an expansion rack but you will not be able to use
the ethernet based IO modules such as HART and SCAIME. 




R-71117
Was this helpful?
What can we do to improve the information ?