Technical FAQs

Ask a Question

Preventa XU - What is the time of availability to power of the XUSL4E light curtains

For all the XUSL4E light curtain range, the time of availability to power, is 2 seconds when it is configurated in automatic start. This time is indicated into the user manual. Same time for the XUSL2E light curtains.
Was this helpful?
What can we do to improve the information ?