Technical FAQs

Ask a Question

How do you reset the M340 BMXNOE01x0 module ?

Title
Reset the M340 BMXNOE01x0 module
 
Issue
Reset the M340 BMXNOE01x0 module
 
Product Line
M340, BMXNOE0100, BMXNOE0110

Environment
Unity Pro
 
Cause
N/A
 
Resolution
 In the ethernet port IO DDT (T_COM_ETH_BMX) there is a ETH_RESET command.

Just toggling the bit in an animation table or user code will not cause an M340 Ethernet port to reset.
This requires the use of the WRITE_CMD block in user code.  
What you would do is:

1. Set the Reset bit to 1
2. Execute the WRITE_CMD block in user code
3. Clear the Reset bit in user code
 
Was this helpful?
What can we do to improve the information ?