Technical FAQs

Ask a Question

What is included in the BMEH582040K kit?

Part number BMEH582040K is a kit that is made of two BMEH582040 M580 HSBY processors and two 490NAC0100 HSBY SFP socket to RJ45 adapters.
Was this helpful?
What can we do to improve the information ?