Technical FAQs

Ask a Question

In Somachine, is there a way to STOP/START the M251 Modbus TCP IO Scanner?

Issue:
In Somachine, is there a way to STOP/START the Modbus TCP IO Scanner through logic?

Product Line:
M251, MB/TCP IO Scanning

Environment:


Cause:


Resolution:
Yes, there are two function blocks in the Somachine Modbus TCP IOScanner library called IOS_STOP and IOS_START which will stop/start the IO Scanner.
 
Was this helpful?
What can we do to improve the information ?