Technical FAQs

Ask a Question

Osisense XC - Datasheet of the adapted switch XCKP2853P16SG2

The XCKP2853P16SG2 adapted switch is the assembly of the following sub-assemblies :
- ZCP28 contact body 2NO slow break,
- ZCE05 rotary head,
- ZCY53 rod lever,
- ZCPEP16 cable gland entry M16x1.5
Please have a look at the attached description.
Was this helpful?
What can we do to improve the information ?