Technical FAQs

Ask a Question

What causes Concept error 'No object found for online read'?

This can occur if you are selecting the 'Read all boolean variables' icon rather than the 'Read all selected variables' icon. 

If you try to animate a block or section that has no true Boolean inputs or outputs, Concept will also display this message.

If animating only one block presents this error, delete the block & re-enter it.  

The customer could also be selecting a section of code that does not have any true BOOLs
Was this helpful?
What can we do to improve the information ?