Technical FAQs

Ask a Question

ION Setup crashes while viewing real-time data from an ACM 3300 meter

ION Setup 3.0 crashes with a "Run-Time Check Failure" error while a user is attempting to view real-time data from an ACM 3300 meter.

Product Line
ION Setup 3.0

ION Setup 3.0

This issue was caused by the use of variable 'ObjAddr' without being initialized. A different version of the compiler was not initializing the variable to zero and therefore it was crashing when working with uninitialized values. 


The issue has been addressed in a subsequent release of ION Setup where the variable 'ObjAddr' was initialized to zero. Ensure that you are running ION Setup v3.0.16071.01 or later.

The latest version of ION Setup may be downloaded from here.
Was this helpful?
What can we do to improve the information ?