Technical FAQs

Ask a Question

Vista Diagram Displaying Incorrect Phase Link and Label for ION6200 Two-Wire Mode

Issue
The default diagram for the 2-wire mode ION6200 meter is linked an labeled incorrectly for the A-Phase kw.
The diagram displays "kW c" instead of "kW a" and the associated numeric register is linked to the "kW c" register on the meter.




Product Line
ION6200
Power Monitoring Expert 7.2.x/8.0
StruxureWare Power Monitoring 7.0.x
ION Enterprise 6.0.x

Environment
Vista and Web Applications Diagrams

Resolution
The attached ".dgm" file should be placed in the following directory to replace the original.

"...\config\diagrams\ud\default\6200_FAC-2WYE_V1.3.1"




 
Was this helpful?
What can we do to improve the information ?