Technical FAQs

Ask a Question

What causes Concept error: "Sequential download not possible"?

There are sometimes more than one change pending download.
These changes can be downloaded  together or separately and sequentially.
 
A sequential download is a method by which the user can download changes to the running application one change at a time.
This is a preferable way to download changes as it makes better use of free memory than downloading multiple changes all at once.

 
If you make several changes to your project, you can go to the "Download changes" selection.  At this point, you can choose 'download changes' and all sections
will be modified.  However, you can have highlighted a single change, or a couple of the several pending changes simply by highlighting them.

This is a sequential download.  You are downloading changes but choosing to download only a few at a time rather than all the pending changes.
 
 
Was this helpful?
What can we do to improve the information ?