Technical FAQs

Ask a Question

What is the difference between the BME NOC 03xx and the BMX NOC 04xx ?

The BME NOC 03xx is identical to the BMX NOC 04xx from a functionality standpoint. The BME NOC03xx is different in that it's Interlink port has
been moved to the back of the module which allows it to communicate over the BME XBP xx00 backplanes to the M580 .

The BMX NOC 04xx are already in use today with M340. 


R-72417
 
Was this helpful?
What can we do to improve the information ?