Technical FAQs

Ask a Question

What are the part numbers for the M580 hot standby CPUs?

The M580 hot standby part numbers are the following:
 
BME H58 20 40
BME H58 40 40
BME H58 60 40
Was this helpful?
What can we do to improve the information ?