Technical FAQs

Ask a Question

What are the replacement for the AGOKIT018M0xx, AGOKIT019M0xx and AGOKIT024M0xx cables?

Issue: Replacement

Product Line: Lexium  BPH Motors

Environment: None

Cause: Obsolescence

AGOKIT018M0xx is the power cable for for teh BPH075x, BPH 095x and PBPH115x series motors and AGOKIT024M0xx is the resolver cable.
AGOKIT024M0xx is the power cable and AGOKIT019M0xx is the resolver cable  respectively for the BPH14xx and BPH19xx series motors. These cables are obsolete and there are no replacements either.  Making one's own cables probably is an option.

Please see the cable specifications in the attachment.

For Power Cables AGOKIT018M0xx, please refer AGOCAV004 - description in page 2 of the pdf document.

For Power Cables AGOKIT019M0xx, please refer AGOCAV005 - description in page 2 of the pdf document.

For Resolver cable AGOKIT024M0xx, please refer AGOCAV003 - description in page 2 of the pdf document.

The drive side connector for the power cable is a Phoenix connector bearing Phoenix part numbers

Back Shell : KGS-PC4/6-F
Connector : PC-4/6-ST-7.62

The drive side connector for the resolver cable is a DB9 Male connector.with a grounding tab.

The motor side connectors are M23 (resolver) and M40 style (power) connectors.

The following vendor may offer similar cables and connectors.

http://www.rde-usa.com/



 
Was this helpful?
What can we do to improve the information ?