Technical FAQs

Ask a Question

What is the replacement battery for Momentum processors?

The Momentum processor adapters do not have a battery. These processor adapters plug onto the 172JNN/PNN option adapters which then plug onto the I/O base. Only the JNN and PNN option adapters use battery backup. These include the 172JNN21032, 172PNN21022 and 172PNN26022 option adapters. Momentum option adapters with < PV01 used alkaline AAA batteries. Momentum option adapters with PV01 > use lithium 3.6v battery part number 170XTS15000.
Was this helpful?
What can we do to improve the information ?