Technical FAQs

Ask a Question

What is new in the latest OS Image for HMIG5U?

A new OS Image for HMIG5U is available with the following changes:
- Support of the new Intel CPU version (E660->E680) 
- Support of the new CFAST reference
- Install of Internet Explorer 11 (support of HTML5, WebVisu...)
Install of Microsoft redistributable Visual Studio 2013 for VijeoXD
- Updates Fire Wall parameters settings (Inbound rules) for targets download by Ethernet
Add Windows QFE (Quick Fix Engineering) for Touch Screen 

You can download the Image on following link:

To download the Backup Recovery tool:

Was this helpful?
What can we do to improve the information ?