Technical FAQs

Ask a Question

Osisense XC - NRTL certificate (Nationally Recognized Testing Laboratories) for the ZCKJ21 contact body

The ZCKJ21 limit switches are UL and CSA certified. Both UL and CSA laboratories are recognized as NRTL (Nationally Recognized Testing Laboratories) by OSHA. Please refer to the following @
Please find hereafter the corresponding certificates :
- UL certificate (link to on-line certification record)
- CSA certificate in attachment.
Was this helpful?
What can we do to improve the information ?