Technical FAQs

Ask a Question

SBS Upgrades: Saved tabular report loses the source names (Hierarchy nodes) after SBS upgrade. Report still runs

After the SBS (side by side) migration the Tabular report does not display the sources which were selected when it was saved but the report still runs.
See screen shot attached

Product line:
Power Monitoring expert 8.1

Unavailable at the moment of writing of this Resolution.

Select the source button and you will be able to visualize the sources used in the report

Was this helpful?
What can we do to improve the information ?