Technical FAQs

Ask a Question

M580 processor and HART using third party AMS software - IP address is not changeable and stuck at

This is a known issue when selecting the M580 processor in any Asset Management System (PACTware or Field Care) and trying to change the IP address. The work around is to select and use the Ethernet/IP Comm Adapter DTM in place of the M580 processor and you will be able to change the IP and connect to the HART slave device through the M580 BMEAHI0812 HART module.
Was this helpful?
What can we do to improve the information ?