Technical FAQs

Ask a Question

Osisense XC special - What is the difference between the XR2AA02K04 and the XR2AA03K04 screw limit switches

The main difference between the XR2AA02K04 and the XR2AA03K04 screw limit switches, having the same gearbox ratio K*, is the number of C/O contacts inside the enclosure. Both switches use the same enclosure. Please see old catalogue data, giving the contact number for both switches. In the current "Osisense XC special catalogue", the XR2AA02K* references are not shown anymore. Find hereafter the XR2AA02K* switches list, still available to order in 2016 : XR2AA02K04, XR2AA02K08, XR2AA02K10, XR2AA02K20, XR2AA02K3, XR2AA02K40, XR2AA02K6, XR2AA02K80, XR2AA02K560. For the other K* gearbox ratios, replace the XR2AA02K* by the XR2AA03K* available to order.


Was this helpful?
What can we do to improve the information ?