Technical FAQs

Ask a Question

Is there an offer in the TM3 range for resistance analog input?

Issue:
Is there an offer in the TM3 range for resistance analog input?

Product Line:
ohm, resistance, analog input

Environment:


Cause:


Resolution:
Part number TM3TI8T/G will do resistance input from a potentiometer.  The resistance range is between 100 - 32K ohm.
Was this helpful?
What can we do to improve the information ?