Technical FAQs

Ask a Question

What is the Phoenix Contact part number for the power connectors used on LMC20 ?

The Phoenix Contact part number for the 3 position power connector used on LMC20 is Phoenix type is MC 1.5/3-ST-3.81

This connector can be purchased directly from Phoenix Contact or from a third party vendor such as Mouser.  Mouser part number of 651-1803581 
 
http://www.mouser.com/catalog/645/usd/1737.pdf




 
Was this helpful?
What can we do to improve the information ?