Technical FAQs

Ask a Question

Osisense XC - XCKJ10559H29 datasheet

Please find attached the complete limit switch XCKJ10559H29 datasheet. In 2016, it is available to order. It is in stock in our international distribution centers. Composition of this complete limit switch XCKJ10559H29 = ZCKJ1H29 contact body + ZCKE05 rotative head + ZCKY59 rod lever arm (dia 6mm, thermoplastic). Note that this head is not positive (not rigid).
Was this helpful?
What can we do to improve the information ?