Technical FAQs

Ask a Question

Is the ConneXium TSXETG100 Ethernet to Serial Gateway Class 1 Div 2 Compliant?

TSXETG100:
CLASS I, DIVISION 2 COMPLIANT INSTALLATION REQUIREMENTS AND WARNINGS
This equipment is suitable for use in Class I, Division 2, Groups A, B, C, and D or non-hazardous locations only.
Was this helpful?
What can we do to improve the information ?