Technical FAQs

Ask a Question

Can the new Backplanes BMEXBPxx02 and the redundant power supply BMXCPS4002 be used with M340 racks.

You can have the Redundant PS with the M340 rack plugged in, but because the M340 cannot use the Ethernet backplane, the M340 will not be able to know if redundancy is ok or not. You will need to wire each PS relay to an input module
Was this helpful?
What can we do to improve the information ?