Technical FAQs

Ask a Question

In the Network Time Service Diagnostics screen, why is there a green bullet switching between primary and secondary NTP Server addresses ?

This is the behaviour of the diagnostics screen when the CPU is set as NTP client and none of the two servers is available. You should fix the issue of the NTP servers, or the network path to these servers.
Was this helpful?
What can we do to improve the information ?