Technical FAQs

Ask a Question

When I add a Quantum drop ( 140CRA ) under M580 CPU, I get a popup saying there is not appropriate drop adapter available while using Unity Pro V11

In UnityPro V11.0, the support of 140CRA was disabled intially.
To enable the support of 140CRA and quantum drops, please instal the hotfix V11 HF1, that can be found on
Was this helpful?
What can we do to improve the information ?