Technical FAQs

Ask a Question

If a modification is done offline, even a online modification, if the project is build, then reconnect to the M580 HSBY PLC the system will not be redundant anymore while using Unity Pro V11

In order to master the modification offline of a redundant HSBY system, use the "virtual connected" mode option in Unity Pro
Was this helpful?
What can we do to improve the information ?