Technical FAQs

Ask a Question

The Time zone is UTC-12 but not UTC+8 when the PC OS is Chinese Win Server 2012 OS

When Win Server 2012 is installed in Chinese, the time zone displayed by default is UTC-12:00 instead of UTC+08:00.
It is recommended to change the time zone from UTC-12:00 to UTC+08:00 entering a custom time zone.
Was this helpful?
What can we do to improve the information ?